AOUT#.SOURCE
Description
This keyword sets the source of the analog output
| Value | Description |
|---|---|
| 0 | AOUT#.VALUE is driven by AOUT#.VALUEU. |
| 1 | AOUT#.VALUE can be driven by an action in the Action table |
Examples
Usage
When AOUT#.SOURCE = 0 (User), then AOUT #.VALUE will be controlled by AOUT #.VALUEU.
When AOUT #.SOURCE = 1 (Action table), then AOUT #.VALUE will be controlled by the assigned action, if any.
Code
Changing output value with VALUEU and then changing SOURCE to be action table with no action configured:
--> AOUT1.SOURCE 0 (User) --> AOUT1.VALUE 0.000 V --> AOUT1.VALUEU 1 --> AOUT1.VALUE 1.000 V --> AOUT1.SOURCE 1 --> AOUT1.VALUE 0.000 V
Context
For more information see Analog Output.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
|
Copyright © 2018 Kollmorgen |
|